No access to FRMD-K64F-Board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

No access to FRMD-K64F-Board

1,880 次查看
j_oberfell
Contributor I

I use FRDM k64f-Board and the demo application is running without problems.

The problem ist, that i have no access to the board.

MBED driver is installed like descriptionin the quick start guide.

I see the MBED USB device, but if i click on it, a error message "access denied" appears.

0 项奖励
回复
2 回复数

1,627 次查看
adriancano
NXP Employee
NXP Employee

Hi,

As Michal said you need to use the Segger J-Link OpenSDA v2 firmware, this is one of the ways to use the FRMD-K64. You may find useful these links:

Segger J-Link Firmware for OpenSDAv2 | MCU on Eclipse

http://developer.mbed.org/handbook/Firmware-FRDM-K64F

Recovering FRDM-K64F mbed Board | MCU on Eclipse

I hope this information can help you.

Regards,

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. It would be nice!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,627 次查看
mike_susen
NXP Employee
NXP Employee

Hi Joachim,

You can burn into freedom board J-Link OPENSDA firmware from segger's web pages: SEGGER - The Embedded Experts - OpenSDA / OpenSDA V2

If you can use segger's OSDA, you must use version 2. Version 2.1 doesn't work with frdm-k64f.

Michal

0 项奖励
回复