No SPI Chip Select option in SynchroMaster component of Processor Expert for K60DN512xxx10 MCU

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

No SPI Chip Select option in SynchroMaster component of Processor Expert for K60DN512xxx10 MCU

1,688 Views
dkarthik
Contributor II

Hi,

There is no chipselect option in the SynchroMaster Component. It uses Serial Master LDD Component internally in which the chipselect is set to 0. Does anyone know how to enable and set pin for chipselect in the SynchroMaster component?

Thank you,

Karthik

chipselect.PNG.pngchipselect.PNG.png

     This is SynchroMaster Component Properties                                                                                                              It internally uses LDD SPI Master component in which there is chip select = 0

Labels (1)
Tags (3)
1 Reply

1,462 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

hello Karthik,

please use SPIMaster_LDD which can do chip select.

=================================================

this answer is for you, if it helps, please click on "correct answer" button. thanks!

Best Regards,

ZhangJun

0 Kudos
Reply