No SDK support for FRDM-KE04Z or KE04Z?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

No SDK support for FRDM-KE04Z or KE04Z?

2,270件の閲覧回数
dstraight
Contributor II

Hi,

Using this link:

https://mcuxpresso.nxp.com/en/select 

I was unable to find the

FRDM-KE04 

or its processor

KE04

I've Tried a few search strings such as - KE04, MKE04, and  MKE04Z8

Is there an SDK for the MKE04Z8 (or the Freedom Board)?   

David

Screen Shot 2017-02-17 at 7.21.06 AM.png

2 返答(返信)

1,998件の閲覧回数
MarekTrmac
NXP Employee
NXP Employee

Hi David,

based on document located here: https://community.nxp.com/docs/DOC-333073 it seems SDK support is not planned.

Regards

Marek

1,998件の閲覧回数
mjbcswitzerland
Specialist V

Hi

http://www.utasker.com/kinetis.html

This supports almost all parts, including KE04, with device simulation and the ability to essentially run the same code on a KE04 up to a K70 without porting effort.

Regards

Mark

0 件の賞賛
返信