New Freedom FRDM-K64F board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

New Freedom FRDM-K64F board

1,645 Views
mjbcswitzerland
Specialist V

Hi All

The new Freedome board was unveiled today at FTF Americas. Costing about $29 it is packed full of features:

  • Freescale K64F Kinetis K64 MCU (MK64FN1M0VLL12)
    • High performance ARM® Cortex™-M4 Core
    • 120MHz, 256KB RAM, 1MB FLASH
    • SPI (3)
    • I2C (3)
    • UART (6)
    • USB OTG / Host / Device
    • USB
    • PWM
    • ADC (2x 16bit with mux)
    • DAC (2x 12bit)
    • Touch Sensor
    • GPIO

FRDM-K64F Onboard Additions

  • FXOS8700CQ - 3-axis accelerometer and magnetometer
  • Ethernet
  • 2 push buttons
  • RGB LED

Full details are at FRDM-K64F: Freescale Freedom Development Platform for Kinetis K64, K63, and K24 MCUs

The uTasker proejct has been ported to this new board and a simulation is already available as discussed here: New Freedom FRDM-K64F board

Regards

Mark

Tags (2)
0 Kudos
Reply
0 Replies