Need the BSDL file for the MK20DN512VLL10

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Need the BSDL file for the MK20DN512VLL10

ソリューションへジャンプ
5,106件の閲覧回数
Larry5335
Contributor IV

Please post the BSDL file for the MK20DN512VLL10.

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
4,508件の閲覧回数
Larry5335
Contributor IV

Here is the link to the BSDL file for this part:

k20_100mhz_100lqfp_14x14_xm33z_xn30d.bsdl.zip

元の投稿で解決策を見る

8 返答(返信)
4,505件の閲覧回数
Larry5335
Contributor IV

Here is the file for the 121 ball BGA package.

0 件の賞賛
返信
4,504件の閲覧回数
zohargolan
Contributor III

Thank you Larry,

I ended up using the attached BSDL instead

0 件の賞賛
返信
4,504件の閲覧回数
zohargolan
Contributor III

Hi Iva, Chris,

 

Can you also provide the BSDL file for MK20dn512vmc10. I've asked for it lask week and got no response. I am really stuck right now.

 

Please help,

Zohar

0 件の賞賛
返信
4,509件の閲覧回数
Larry5335
Contributor IV

Here is the link to the BSDL file for this part:

k20_100mhz_100lqfp_14x14_xm33z_xn30d.bsdl.zip

4,504件の閲覧回数
cguarneri
NXP Employee
NXP Employee

Larry,

The BSDL file was sent to you.

0 件の賞賛
返信
4,504件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Hi Larry,

Sure. Give me short time for get it.

Best Regards,

Iva

0 件の賞賛
返信
4,504件の閲覧回数
Larry5335
Contributor IV

Iva,

Any idea how much longer for the file?

0 件の賞賛
返信
4,504件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Hello Larry,

I got the same file as Christopher.

In case of some problems, contact us.

Best Regards,

Iva

0 件の賞賛
返信