Need the BSDL file for the MK20DN512VLL10

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Need the BSDL file for the MK20DN512VLL10

Jump to solution
3,427 Views
Larry5335
Contributor IV

Please post the BSDL file for the MK20DN512VLL10.

Labels (1)
Tags (3)
0 Kudos
Reply
1 Solution
2,829 Views
Larry5335
Contributor IV

Here is the link to the BSDL file for this part:

k20_100mhz_100lqfp_14x14_xm33z_xn30d.bsdl.zip

View solution in original post

8 Replies
2,826 Views
Larry5335
Contributor IV

Here is the file for the 121 ball BGA package.

0 Kudos
Reply
2,825 Views
zohargolan
Contributor III

Thank you Larry,

I ended up using the attached BSDL instead

0 Kudos
Reply
2,825 Views
zohargolan
Contributor III

Hi Iva, Chris,

 

Can you also provide the BSDL file for MK20dn512vmc10. I've asked for it lask week and got no response. I am really stuck right now.

 

Please help,

Zohar

0 Kudos
Reply
2,830 Views
Larry5335
Contributor IV

Here is the link to the BSDL file for this part:

k20_100mhz_100lqfp_14x14_xm33z_xn30d.bsdl.zip

2,825 Views
cguarneri
NXP Employee
NXP Employee

Larry,

The BSDL file was sent to you.

0 Kudos
Reply
2,825 Views
ivadorazinova
NXP Employee
NXP Employee

Hi Larry,

Sure. Give me short time for get it.

Best Regards,

Iva

0 Kudos
Reply
2,825 Views
Larry5335
Contributor IV

Iva,

Any idea how much longer for the file?

0 Kudos
Reply
2,825 Views
ivadorazinova
NXP Employee
NXP Employee

Hello Larry,

I got the same file as Christopher.

In case of some problems, contact us.

Best Regards,

Iva

0 Kudos
Reply