Need th schematic of MED-GLU AFE.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Need th schematic of MED-GLU AFE.

Jump to solution
4,793 Views
joicemarkose
Contributor II

i am  planning to develop a glucose meter with the tower kit of freescale.

But the AFE for developing the same, MED-GLUE is unavailable in the market.i am  hoping to develop the PCB once  i have the gerber file of the same.

If its possible, please help me get the gerber file necessary for developing MED-GLU AFE.

what type of test strips should i use with this ? any particular one available in the market

thank you in advance for spending your valuable time.

1 Solution
4,358 Views
santiago_lopez
NXP Employee
NXP Employee

Hi Joice,

Gerber files can be found together with the fimware for the AppNote AN4364 in the file AN4364SW.zip in the NXP web page. I'm attaching those files to this thread.

Hope it helps.

Saludos

View solution in original post

5 Replies
3,006 Views
Constance
Contributor I

As a fellow tinkerer, I totally relate to your quest for the elusive MED-GLUE! It’s like searching for a unicorn in a tech jungle. If only Google could conjure up that Gerber file with a simple search! As for test strips, I’d suggest looking for ones compatible with your meter—think of them as the perfect sidekick to your glucose adventure. Good luck, and may your PCB dreams come true!

0 Kudos
Reply
4,358 Views
joicemarkose
Contributor II

Thanks a lot Santiago,

i found it really helpful. It would much appreciated if you could give some tech details of strips to be used along this module.

0 Kudos
Reply
4,358 Views
santiago_lopez
NXP Employee
NXP Employee

Hi Joice,

Sure, please send me a personal message to share that information with you. Click on the pencil icon next to your user name and select "Message". Then find my profile under the name Santiago_Lopez.

Saludos

0 Kudos
Reply
3,013 Views
Nikunj_Solanki
Contributor III

I hope you are doing well. I am currently working with a multi-monitor glucose meter and would like to get more details on the compatible strips that can be used along with it. Specifically, I would appreciate information on:

  • Recommended strip models and specifications
  • Interface and compatibility details
  • Any relevant documentation or application notes

Please let me know if you need any additional details from my end. Looking forward to your response.

Best regards,

Tags (1)
0 Kudos
Reply
4,359 Views
santiago_lopez
NXP Employee
NXP Employee

Hi Joice,

Gerber files can be found together with the fimware for the AppNote AN4364 in the file AN4364SW.zip in the NXP web page. I'm attaching those files to this thread.

Hope it helps.

Saludos