Need help with k70

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Need help with k70

1,224件の閲覧回数
sudeepaithal
Contributor I

Hello,can anyone please tell me if k70 MCU can deliver 3.3V signal from one pin(I/O pin) and 1.8v signal from another pin(I/O pin) simultaneously?If yes then which register should be access to make the necessary changes.

0 件の賞賛
返信
1 返信

1,107件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

For K70 has two DAC modules, customer can use one DAC module output 3.3V voltage and another DAC module output 1.8V voltage.

The K70 is single voltage powered, if customer using VDD 3.3V, then customer also could use one GPIO pin output 3.3V voltage and using a DAC module output 1.8V voltage.

Wish it helps.

best regards,

Ma Hui

0 件の賞賛
返信