Need help with k70

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Need help with k70

809 次查看
sudeepaithal
Contributor I

Hello,can anyone please tell me if k70 MCU can deliver 3.3V signal from one pin(I/O pin) and 1.8v signal from another pin(I/O pin) simultaneously?If yes then which register should be access to make the necessary changes.

0 项奖励
回复
1 回复

692 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

For K70 has two DAC modules, customer can use one DAC module output 3.3V voltage and another DAC module output 1.8V voltage.

The K70 is single voltage powered, if customer using VDD 3.3V, then customer also could use one GPIO pin output 3.3V voltage and using a DAC module output 1.8V voltage.

Wish it helps.

best regards,

Ma Hui

0 项奖励
回复