Need basic K60 example project using DMA transfer LDD

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Need basic K60 example project using DMA transfer LDD

ソリューションへジャンプ
2,358件の閲覧回数
steve_fae
Senior Contributor I

The TIC sent me an example but its a bit too complicated.  I have never used DMA so looking to see an example of moving some data out SPI using DMA. 

ラベル(1)
タグ(4)
0 件の賞賛
返信
1 解決策
1,681件の閲覧回数
Monica
Senior Contributor III

Steven, if the custom examples provided by the experts are too much to start with, check out this site FreeRTOS demo for the Kinetis K60 Cortex-M4 based microcontroller - including an embedded web server...

Keep us posted! :smileywink:

Regards

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,682件の閲覧回数
Monica
Senior Contributor III

Steven, if the custom examples provided by the experts are too much to start with, check out this site FreeRTOS demo for the Kinetis K60 Cortex-M4 based microcontroller - including an embedded web server...

Keep us posted! :smileywink:

Regards

0 件の賞賛
返信