Need basic K60 example project using DMA transfer LDD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Need basic K60 example project using DMA transfer LDD

Jump to solution
2,451 Views
steve_fae
Senior Contributor I

The TIC sent me an example but its a bit too complicated.  I have never used DMA so looking to see an example of moving some data out SPI using DMA. 

Labels (1)
Tags (4)
0 Kudos
Reply
1 Solution
1,774 Views
Monica
Senior Contributor III

Steven, if the custom examples provided by the experts are too much to start with, check out this site FreeRTOS demo for the Kinetis K60 Cortex-M4 based microcontroller - including an embedded web server...

Keep us posted! :smileywink:

Regards

View solution in original post

0 Kudos
Reply
1 Reply
1,775 Views
Monica
Senior Contributor III

Steven, if the custom examples provided by the experts are too much to start with, check out this site FreeRTOS demo for the Kinetis K60 Cortex-M4 based microcontroller - including an embedded web server...

Keep us posted! :smileywink:

Regards

0 Kudos
Reply