Need basic K60 example project using DMA transfer LDD

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Need basic K60 example project using DMA transfer LDD

跳至解决方案
2,396 次查看
steve_fae
Senior Contributor I

The TIC sent me an example but its a bit too complicated.  I have never used DMA so looking to see an example of moving some data out SPI using DMA. 

标签 (1)
标记 (4)
0 项奖励
回复
1 解答
1,719 次查看
Monica
Senior Contributor III

Steven, if the custom examples provided by the experts are too much to start with, check out this site FreeRTOS demo for the Kinetis K60 Cortex-M4 based microcontroller - including an embedded web server...

Keep us posted! :smileywink:

Regards

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,720 次查看
Monica
Senior Contributor III

Steven, if the custom examples provided by the experts are too much to start with, check out this site FreeRTOS demo for the Kinetis K60 Cortex-M4 based microcontroller - including an embedded web server...

Keep us posted! :smileywink:

Regards

0 项奖励
回复