Need Keil uvision sample projects for FRDM-KL25Z

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Need Keil uvision sample projects for FRDM-KL25Z

4,010件の閲覧回数
sunnyraut
Contributor I

Want to design data logger using FRDM KL25Z, hence need "keil uvision" sample projects to start with development using "keil MDK 5".

Also need keil project to read,write an modify file using OTG functionality. Aim requirement is to store data in pendrive.

Send me Sample projects if possible else suggest me where I can find them.

0 件の賞賛
返信
3 返答(返信)

3,213件の閲覧回数
mjbcswitzerland
Specialist V

Hi

http://www.utasker.com/kinetis/FRDM-KL25Z.html

This includes a complete Keil uVision project with utFAT on pen-drive with data logging of sampled ADC values, which is also simulated in VisualStudio (including the pen-drive).

Regards

Mark

Kinetis for professionals: http://http://www.utasker.com/kinetis.html

0 件の賞賛
返信

3,214件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Hi Sunny.

Please, check KSDK sample projects also for Keil. Software Development Kit for Kinetis MCUs|NXP 

KSDK 2.0 was tested on MDK-ARM Microcontroller Development Kit (Keil)® 5.18a

The package for FRDM-KL25Z you can download from Welcome to Kinetis Expert | Kinetis Expert 

You will find USB examples under c:\Freescale\KSDK 2.0\SDK_2.0_FRDM-KL25Z\boards\frdmkl25z\usb_examples\

I hope this helps you.

Best Regards,

Iva

0 件の賞賛
返信

3,214件の閲覧回数
sunnyraut
Contributor I

Thank you IVA

I appreciate

On Tue, Sep 13, 2016 at 7:07 PM, ivadorazinova <

0 件の賞賛
返信