NXP FRDM-K64 Users Guide Misleading Pinout Information - BT J199 Connector

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP FRDM-K64 Users Guide Misleading Pinout Information - BT J199 Connector

2,196 Views
datamstr
Contributor II

Hello NXP,

I am not sure if this is the right place to report this since the Service Request system has been changed.

In the FRDM-K64F Freedom Module User’s Guide on Page 19, I noticed that there is misleading information for the BT J199 header pinout.  The text location really should be reversed since Pin 1 is on the left.

Document Number: FRDMK64FUG User’s Guide

Rev. 0.1, 04/2014

(See attached picture, yellow mark is pin 1)

Thanks,

David

Tags (1)
0 Kudos
Reply
1 Reply

2,032 Views
miduo
NXP Employee
NXP Employee

Hi,

You are right, the J199 header numbers are mirrored in that card. We apologize for this inconvenience, which could cause connection problems. Actually we had reported this document error 1 years ago and it will been corrected in next version.

B.R.

Fang

0 Kudos
Reply