NVM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NVM

2,104 Views
ravibhatt
Contributor I

hey guyz !

how to fix the error showing `undefined referenced to __start_NVM_TABLE' in NV_flash.c file when I do enable(1) to #define gNvStorageIncluded_d   1. Due to this error I am unable to store BLE bonding information in NVM region in MKW41Z512 nxp controller. ???

0 Kudos
Reply
1 Reply

2,092 Views
nxf56274
NXP Employee
NXP Employee

Hi,

Sometimes it will happen. You can delete your project and export your example again.

Which example do you use? Version of sdk and mcuxpresso?

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply