NMI_b

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NMI_b

1,322 Views
karanchaudhary
Contributor I

Hi,

I am working on KEAZ8(16 Pin) microcontroller and the IDE is Codeworrier 10.6.4.

I want to use Pin no-8: NMI_b/PTB4/FTM2_CH4 as a timer channel in input capture

mode. But when i connect this pin to the hardware, my hardware does not connect

with debugger (U-Multilink) and indicate error. Please help me.

Labels (1)
0 Kudos
Reply
1 Reply

1,199 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Alok,

Actually after have a brief look through your description above, I'm still not very clear with your question.

So I'd like to confirm some points with you.

1. Can you share the sch of the debug interface?

2. I'm also very curious about what exactly error you encountered, can you please illustrate the screenshot of the error message?

I'm looking forward to your reply.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply