NMI_b

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NMI_b

1,386件の閲覧回数
karanchaudhary
Contributor I

Hi,

I am working on KEAZ8(16 Pin) microcontroller and the IDE is Codeworrier 10.6.4.

I want to use Pin no-8: NMI_b/PTB4/FTM2_CH4 as a timer channel in input capture

mode. But when i connect this pin to the hardware, my hardware does not connect

with debugger (U-Multilink) and indicate error. Please help me.

ラベル(1)
0 件の賞賛
返信
1 返信

1,263件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Alok,

Actually after have a brief look through your description above, I'm still not very clear with your question.

So I'd like to confirm some points with you.

1. Can you share the sch of the debug interface?

2. I'm also very curious about what exactly error you encountered, can you please illustrate the screenshot of the error message?

I'm looking forward to your reply.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信