My computer shutdown randomly (not always) when connecting KL25Z USB on my MacBookPro

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

My computer shutdown randomly (not always) when connecting KL25Z USB on my MacBookPro

3,905件の閲覧回数
lucasmahieu
Contributor III

Hello,

I am using the FRDM KL25Z on my macbook pro.

I also use VirtualBox to use windows, and code warrior.

All works fine, but some times juste when i connect the USB cable, my computer freeze during 3 secondes, and shut down, then restart.

Doest some other people had this strange issue ?

Or do you have an idea of the reason ?

REGARDS

0 件の賞賛
返信
10 返答(返信)

3,618件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

We don't have record about similar issue.

What kind of USB function of FRDM-KL25Z board?

Could you change using another USB port of Macbook pro? If both USB ports could cause the same phenomenon?


Wish it helps.

Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,618件の閲覧回数
lucasmahieu
Contributor III

Hey,

Thank for your quick response,

I change the Frdm for a very New one ... And a always have the same problem ...

I also tried all my Usb port , and it was the same...

I use the openSDA of the kl25z.

Regards

Le 1 avr. 2016 à 05:07, Hui_Ma <[email protected]> a écrit :

NXP Community

My computer shutdown randomly (not always) when connecting KL25Z USB on my MacBookPro

reply from Hui_Ma in Kinetis Microcontrollers - View the full discussion

Hi

We don't have record about similar issue.

What kind of USB function of FRDM-KL25Z board?

Could you change using another USB port of Macbook pro? If both USB ports could cause the same phenomenon?

Wish it helps.

Have a great day,

Ma Hui

0 件の賞賛
返信

3,618件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

Sorry for the so later reply.

I would recommend customer update the OpenSDA firmware with Segger provided J-Link firmware.

I checked there with description that :

Due to limitations of the OpenSDA bootloader replacing the firmware to use it as a J-Link can only be done on Windows and Linux systems. When the firmware is replaced, it can be used like any J-Link on Mac OS/X, too.

More detailed info, please check below link:

SEGGER - The Embedded Experts - OpenSDA / OpenSDA V2


Wish it helps.

Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,618件の閲覧回数
lucasmahieu
Contributor III

Thanks a lot , it is a very good news, i will try it now.

So i have to change the boot loader of the KL25z board ?

do you knew where i can download the «

Segger provided J-Link firmware »

thanks again

regards

0 件の賞賛
返信

3,618件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

No need to change the bootloader image.

Please refer below picture to update the OpenSDA firmware to J-Link firmware:

2016-04-05_17-20-53.jpg


Wish it helps.

Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,618件の閲覧回数
lucasmahieu
Contributor III

Hi,

I did it this morning, and now i see a "j-link" devis on my destop,

But how a can put my programm .srec or .hex in the frdm ?

Le 5 avr. 2016 à 11:23, Hui_Ma <[email protected]> a écrit :

NXP Community

My computer shutdown randomly (not always) when connecting KL25Z USB on my MacBookPro

reply from Hui_Ma in Kinetis Microcontrollers - View the full discussion

Hi

No need to change the bootloader image.

Please refer below picture to update the OpenSDA firmware to J-Link firmware:

Wish it helps.

Have a great day,

Ma Hui

0 件の賞賛
返信

3,618件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

Do you have the IDE software?

You could using J-Link to debug the code, which will program the KL25 Flash before debugging.


Wish it helps.

Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,618件の閲覧回数
lucasmahieu
Contributor III

Hi

Yes i use KDS

I will try to flash and to run a program soon.

I will give you news if my problem persist

0 件の賞賛
返信

3,618件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

Please let us know if there still with debug issue. Thanks.


Wish it helps.

Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,618件の閲覧回数
lucasmahieu
Contributor III

Hi

I am realy sorry, but i still have the bug...

I can flash the board, bus about 1 time on 10 my computer shit down ...

I am rely sorty for you, cause you gave me realy good information .

I hop i will find the cause of the issue

Regards

Le 7 avr. 2016 à 04:48, Hui_Ma <[email protected]> a écrit :

NXP Community

My computer shutdown randomly (not always) when connecting KL25Z USB on my MacBookPro

reply from Hui_Ma in Kinetis Microcontrollers - View the full discussion

Hi

Please let us know if there still with debug issue. Thanks.

Wish it helps.

Have a great day,

Ma Hui

0 件の賞賛
返信