Must USB clock source be 48MHz clock on USB-KW24D512?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Must USB clock source be 48MHz clock on USB-KW24D512?

1,138件の閲覧回数
luwan
Contributor II


Can this 20~25MHz clock after start-up be used for driving USB driver?

If 20~25MHz is not large enough, can we scale the clock to 48MHz via configuring MCG_C4, but still keep running in FEI mode?

ラベル(2)
0 件の賞賛
返信
1 返信

977件の閲覧回数
miduo
NXP Employee
NXP Employee

Hi,

No, you can not do that. The USB clock should be 48MHz and as I had mentioned that we do not recommend to use FLL to clock the USB.

0 件の賞賛
返信