Multiplication 1 cycle and division 3 cycles with Floating point Unit?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Multiplication 1 cycle and division 3 cycles with Floating point Unit?

跳至解决方案
3,934 次查看
BasePointer
Contributor II

Hi,

 

Yesterday I have watched a video related with kinetis introduction on freescale web page.

 

There, they said floating point multiplication is 1 cycle, and floating point division is 3 cycles (something like that, I couldn’t remember the exact values now)

 

As I know, floating point multiplication and division should be same. Aren’t they? I mean dividing a value into 4 is same operation with multiplying it with 0.25? Why are their cycles different?

 

Thanks.

 

0 项奖励
回复
1 解答
3,645 次查看
kef
Specialist I

No, FP multiplication and division aren't the same. You can replace /4 by *0.25, but you can do this only for known constants. You (and not your MCU) calculate reciprocal of divider and use multiplication instead of division. But who will calculate reciprocal of variable to replace division with multiplication? Also, C compiler is not allowed to optimize any FP operation, like replacing division by constant with multiplication by constant, since these can produce not exactly the same results.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
3,646 次查看
kef
Specialist I

No, FP multiplication and division aren't the same. You can replace /4 by *0.25, but you can do this only for known constants. You (and not your MCU) calculate reciprocal of divider and use multiplication instead of division. But who will calculate reciprocal of variable to replace division with multiplication? Also, C compiler is not allowed to optimize any FP operation, like replacing division by constant with multiplication by constant, since these can produce not exactly the same results.

0 项奖励
回复
3,645 次查看
BasePointer
Contributor II

Yes you are right, thanks :smileyhappy:

0 项奖励
回复