Mkl16Z32 and TSS library

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Mkl16Z32 and TSS library

1,806 次查看
davidra7
Contributor I

Hi All,

I am using mkl16z32 and add tss component and finally it worked for my design but the code size is 18K out of 32K, is there any way to make it smaller ?

I tried to optimize the code and it reduced it to 15K, Any Ideas ?

Also , Tried it on FRDM-KL26Z and I have the same issue.

Thanks,

David

0 项奖励
回复
2 回复数

1,675 次查看
davidra7
Contributor I

Any Help ?

0 项奖励
回复

1,675 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

Hi David

Unfortunatelly the TSS library use around 18 to 20 K

Please check the following thread

Memory requirement for TSS 3.1 library.

I hope this will help you

regards

Vicente Gomez

0 项奖励
回复