Mkl16Z32 and TSS library

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Mkl16Z32 and TSS library

1,811件の閲覧回数
davidra7
Contributor I

Hi All,

I am using mkl16z32 and add tss component and finally it worked for my design but the code size is 18K out of 32K, is there any way to make it smaller ?

I tried to optimize the code and it reduced it to 15K, Any Ideas ?

Also , Tried it on FRDM-KL26Z and I have the same issue.

Thanks,

David

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

1,680件の閲覧回数
davidra7
Contributor I

Any Help ?

0 件の賞賛
返信

1,680件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

Hi David

Unfortunatelly the TSS library use around 18 to 20 K

Please check the following thread

Memory requirement for TSS 3.1 library.

I hope this will help you

regards

Vicente Gomez

0 件の賞賛
返信