Minimum VDD for USB device

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Minimum VDD for USB device

1,531 次查看
jh0
Contributor IV

What is minimum voltage for MKL27Z64VLH4 (or similar M0+) to work as USB device? Is it possible to use it as 1.8V like on attached picture?

If I understood right, during working as crystalless USB device, internal precise 48 MHz clock can be used also as source for master (or for other peripherals) clock. 

I found FlexIO AN for UART, I2C, SPI, PWM. Is there any FlexIO SWD (master) open source example?

标签 (1)
0 项奖励
回复
2 回复数

1,378 次查看
bobpaddock
Senior Contributor III

If communicating via USB the minimum voltage per the standard is 4.2V for VBus.

http://www.usb.org/developers/docs/whitepapers/power_delivery_motherboards.pdf

I know you said Device, understating the Host end is important as well.

http://www.usb.org/developers/compliance/electrical_tests/USB_2_0_Electrical_Compliance_Specificatio...

See http://www.usb.org for others.

0 项奖励
回复

1,378 次查看
miduo
NXP Employee
NXP Employee

Hi,

yes, the internal USB regulator powers the USB transceiver or the MCU itself (depending on the application). 
in this case the supply voltage for chip could be 1.8V.  
0 项奖励
回复