Minimum VDD for USB device

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Minimum VDD for USB device

2,333 Views
jh0
Contributor IV

What is minimum voltage for MKL27Z64VLH4 (or similar M0+) to work as USB device? Is it possible to use it as 1.8V like on attached picture?

If I understood right, during working as crystalless USB device, internal precise 48 MHz clock can be used also as source for master (or for other peripherals) clock. 

I found FlexIO AN for UART, I2C, SPI, PWM. Is there any FlexIO SWD (master) open source example?

Labels (1)
0 Kudos
Reply
2 Replies

2,180 Views
bobpaddock
Senior Contributor IV

If communicating via USB the minimum voltage per the standard is 4.2V for VBus.

http://www.usb.org/developers/docs/whitepapers/power_delivery_motherboards.pdf

I know you said Device, understating the Host end is important as well.

http://www.usb.org/developers/compliance/electrical_tests/USB_2_0_Electrical_Compliance_Specificatio...

See http://www.usb.org for others.

0 Kudos
Reply

2,180 Views
miduo
NXP Employee
NXP Employee

Hi,

yes, the internal USB regulator powers the USB transceiver or the MCU itself (depending on the application). 
in this case the supply voltage for chip could be 1.8V.  
0 Kudos
Reply