Minimum VDD for USB device

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Minimum VDD for USB device

2,404件の閲覧回数
jh0
Contributor IV

What is minimum voltage for MKL27Z64VLH4 (or similar M0+) to work as USB device? Is it possible to use it as 1.8V like on attached picture?

If I understood right, during working as crystalless USB device, internal precise 48 MHz clock can be used also as source for master (or for other peripherals) clock. 

I found FlexIO AN for UART, I2C, SPI, PWM. Is there any FlexIO SWD (master) open source example?

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,251件の閲覧回数
bobpaddock
Senior Contributor IV

If communicating via USB the minimum voltage per the standard is 4.2V for VBus.

http://www.usb.org/developers/docs/whitepapers/power_delivery_motherboards.pdf

I know you said Device, understating the Host end is important as well.

http://www.usb.org/developers/compliance/electrical_tests/USB_2_0_Electrical_Compliance_Specificatio...

See http://www.usb.org for others.

0 件の賞賛
返信

2,251件の閲覧回数
miduo
NXP Employee
NXP Employee

Hi,

yes, the internal USB regulator powers the USB transceiver or the MCU itself (depending on the application). 
in this case the supply voltage for chip could be 1.8V.  
0 件の賞賛
返信