Microprocessor SPI connection

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Microprocessor SPI connection

Jump to solution
1,865 Views
ilginsarican
Contributor II

Hello,
I use MK60DN512VLL10.
I have to use at least 65 ADC data, probably I will use ADS1158 16-Channel, 16-Bit Analog-to-Digital Converter.
I want to know that How many SPIs can hardware connect to the processor's SPI port?

Tags (1)
1 Solution
1,745 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi ılgın sarıcan,

There are three SPI modules on MK60DN512VLL10.
According to the "Table 3-70. SPI PCS signals", you can see there are:
6 PCS signals for SPI0
4 PCS signals for SPI1
1 PCS signals for SPI2

Number of PCS signals.png

Please read "10.3.1 K60 Signal Multiplexing and Pin Assignments" and check if you can arrange all these PCS signals at the same time on your board.

10.3.1 K60 Signal Multiplexing and Pin Assignments.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
1,745 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi ılgın sarıcan,

There are three SPI modules on MK60DN512VLL10.
According to the "Table 3-70. SPI PCS signals", you can see there are:
6 PCS signals for SPI0
4 PCS signals for SPI1
1 PCS signals for SPI2

Number of PCS signals.png

Please read "10.3.1 K60 Signal Multiplexing and Pin Assignments" and check if you can arrange all these PCS signals at the same time on your board.

10.3.1 K60 Signal Multiplexing and Pin Assignments.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------