Microprocessor SPI connection

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Microprocessor SPI connection

ソリューションへジャンプ
1,715件の閲覧回数
ilginsarican
Contributor II

Hello,
I use MK60DN512VLL10.
I have to use at least 65 ADC data, probably I will use ADS1158 16-Channel, 16-Bit Analog-to-Digital Converter.
I want to know that How many SPIs can hardware connect to the processor's SPI port?

タグ(1)
1 解決策
1,595件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi ılgın sarıcan,

There are three SPI modules on MK60DN512VLL10.
According to the "Table 3-70. SPI PCS signals", you can see there are:
6 PCS signals for SPI0
4 PCS signals for SPI1
1 PCS signals for SPI2

Number of PCS signals.png

Please read "10.3.1 K60 Signal Multiplexing and Pin Assignments" and check if you can arrange all these PCS signals at the same time on your board.

10.3.1 K60 Signal Multiplexing and Pin Assignments.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
1,596件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi ılgın sarıcan,

There are three SPI modules on MK60DN512VLL10.
According to the "Table 3-70. SPI PCS signals", you can see there are:
6 PCS signals for SPI0
4 PCS signals for SPI1
1 PCS signals for SPI2

Number of PCS signals.png

Please read "10.3.1 K60 Signal Multiplexing and Pin Assignments" and check if you can arrange all these PCS signals at the same time on your board.

10.3.1 K60 Signal Multiplexing and Pin Assignments.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------