Microcontroller MKM35Z512VLL7 : problems with 2 passes in the Reflow Oven?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Microcontroller MKM35Z512VLL7 : problems with 2 passes in the Reflow Oven?

1,537件の閲覧回数
beste-ivan
Contributor II

Hello to everyone, i'm using th uC MKM35Z512VLL7.


I have a PCB where SMD components are mounted on the top LA and bottom LB sides.
On the TOP side LA, the MKM35Z512VLL7 microcontroller (IC1) is soldered. On the BOTTOM side, a very tall and heavy component is soldered (Relay RL2).
For issues with component (RL2), before we solder the microcontroller IC1 on side LA. Then after we solder component (RL2) on side LB.
Therefore, the microcontroller (IC1) will go through TWO stages in the SMD soldering oven.
The soldering profile is according to the IPC/JEDEC Standard J-STD-020 with T(max)=+260°C.
Can I have problems with the microcontroller if it goes through two cycles in the reflow oven?

 

thanks

Ivan

0 件の賞賛
返信
3 返答(返信)

1,426件の閲覧回数
Veronika_techsupport
NXP TechSupport
NXP TechSupport

Hello @beste-ivan 

could you please contact regarding your issue the point of sale/authorized distributor where you bought your parts? They will be able to check your ordered part and provide you further support. 
Part is MSL 3 level.  https://www.nxp.com/part/MKM35Z512VLL7, https://www.nxp.com/webapp/chemical-content/MKM35Z512VLL7.html
Thank you for understanding.

Best regards

0 件の賞賛
返信

1,467件の閲覧回数
Veronika_techsupport
NXP TechSupport
NXP TechSupport

Hello @beste-ivan 

Your request is currently in progress with responsbile team. Once I will receive response I will come back to you. 

Thank you for your understanding and patience.

Best regards

Kind regards

1,484件の閲覧回数
beste-ivan
Contributor II

Hello everyone. Does anyone have comments or observations on the maximum number of welding cycles that the KM35 can tolerate (one or two)? Tks 

0 件の賞賛
返信