Hi Bill,
Vector table is from address 0X00000000, length is 0XC0:
__Vectors DCD __initial_sp ; Top of Stack
DCD Reset_Handler ; Reset Handler
DCD NMI_Handler ; NMI Handler
DCD HardFault_Handler ; Hard Fault Handler
DCD 0 ; Reserved
DCD 0 ; Reserved
DCD 0 ; Reserved
DCD 0 ; Reserved
DCD 0 ; Reserved
DCD 0 ; Reserved
DCD 0 ; Reserved
DCD SVC_Handler ; SVCall Handler
DCD 0 ; Reserved
DCD 0 ; Reserved
DCD PendSV_Handler ; PendSV Handler
DCD SysTick_Handler ; SysTick Handler
; External Interrupts
DCD Reserved16_IRQHandler ; Reserved interrupt 16
DCD Reserved17_IRQHandler ; Reserved interrupt 17
DCD Reserved18_IRQHandler ; Reserved interrupt 18
DCD Reserved19_IRQHandler ; Reserved interrupt 19
DCD Reserved20_IRQHandler ; Reserved interrupt 20
DCD FTMRE_IRQHandler ; FTMRE command complete/read collision interrupt
DCD LVD_LVW_IRQHandler ; Low Voltage Detect, Low Voltage Warning
DCD IRQ_IRQHandler ; External interrupt
DCD I2C0_IRQHandler ; I2C0 interrupt
DCD I2C1_IRQHandler ; I2C1 interrupt
DCD SPI0_IRQHandler ; SPI0 interrupt
DCD SPI1_IRQHandler ; SPI1 interrupt
DCD UART0_IRQHandler ; UART0 status/error interrupt
DCD UART1_IRQHandler ; UART1 status/error interrupt
DCD UART2_IRQHandler ; UART2 status/error interrupt
DCD ADC0_IRQHandler ; ADC0 interrupt
DCD ACMP0_IRQHandler ; ACMP0 interrupt
DCD FTM0_IRQHandler ; FTM0 Single interrupt vector for all sources
DCD FTM1_IRQHandler ; FTM1 Single interrupt vector for all sources
DCD FTM2_IRQHandler ; FTM2 Single interrupt vector for all sources
DCD RTC_IRQHandler ; RTC overflow
DCD ACMP1_IRQHandler ; ACMP1 interrupt
DCD PIT_CH0_IRQHandler ; PIT CH0 overflow
DCD PIT_CH1_IRQHandler ; PIT CH1 overflow
DCD KBI0_IRQHandler ; Keyboard interrupt 0
DCD KBI1_IRQHandler ; Keyboard interrupt 1
DCD Reserved42_IRQHandler ; Reserved interrupt 42
DCD ICS_IRQHandler ; ICS interrupt
DCD Watchdog_IRQHandler ; WDOG Interrupt
DCD PWT_IRQHandler ; Pulse Width Timer Interrupt
DCD MSCAN_RX_IRQHandler ; MSCAN Rx Interrupt
DCD MSCAN_TX_IRQHandler ; MSCAN Tx, Err and Wake-up interrupt
__Vectors_End
From address 0x400, length X10, it is the flash configuration field.
AREA |.ARM.__at_0x400|, CODE, READONLY
DCB BackDoorK0, BackDoorK1, BackDoorK2, BackDoorK3
DCB BackDoorK4, BackDoorK5, BackDoorK6, BackDoorK7
DCB 0xFF, 0xFF, 0xFF, 0xFF
DCB 0xFF, FPROT, FSEC, FOPT
ENDIF
Other flash address you can used by yourself.
Wish it helps you!
If you still have question about it, please kindly let me know.
Have a great day,
Kerry
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------