Maximum SPI Communication Speed for KM34 at 75 MHz CPU Frequency

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Maximum SPI Communication Speed for KM34 at 75 MHz CPU Frequency

1,289件の閲覧回数
Gohil
Contributor I

Hello NXP Community,

I am currently working with the KM34 microcontroller and running it at a 75 MHz CPU frequency. Could someone please clarify what the maximum SPI communication speed is for this configuration?

Additionally, are there any specific considerations or limitations when configuring SPI on this microcontroller at the 75 MHz CPU frequency? Any recommendations to achieve the highest SPI performance would be greatly appreciated!

Thank you for your support!

0 件の賞賛
返信
1 返信

1,273件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Gohil ,

According to KM34 DS

https://www.nxp.com.cn/docs/en/data-sheet/KM34P144M75SF0.pdf

 

maximum frequency of SPI operation is half of the system clock in master mode.  If you have 75 MHz CPU Frequency, this value is 75/2=37.5 MHz. 

maximum frequency of SPI operation is one-fourth of the system clock in slave mode.  If the CPU Frequency is 75 MHz , this value is 75/4= 18.75 MHz. 

For more about the SPI specification, see above DS, section 3.6.3 SPI switching specifications.

 

Hope this helps,

Jun Zhang

 

 

 

 

 

0 件の賞賛
返信