Maximum NAND Flash memory capacity supported by MK70FN1M0VMJ12

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Maximum NAND Flash memory capacity supported by MK70FN1M0VMJ12

2,466 Views
puspamnayak
Contributor III


Hi,

I want to know what is the maximum memory capacity of NAND Flash will be supported by MK70FN1M0VMJ12

Request you to reply ASAP

Thanks and regards,

Puspam N

Tags (1)
0 Kudos
Reply
4 Replies

2,124 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

NAND Flash is different with NOR Flash, Kineits NAND Flash controller Supports all NAND flash products regardless of density/organization. There with no memory size limited with NAND Flash.


Wish it helps.
best regards
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,124 Views
puspamnayak
Contributor III

Hi Hui,

Thanks for your reply.

I am planning to use 1 Tb NAND Flash.

So as per your explaination NAND Flash controller of K70 will able to address 1 Tb NAND Flash ?

Kindly reply

Thanks and regards,

Puspam Nayak

0 Kudos
Reply

2,124 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Yes, the K70 NAND Flash controller is able to address 1Tb NAND Flash.

It also need the file system to support that  amount size NAND Flash.


Wish it helps.
best regards
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,124 Views
puspamnayak
Contributor III

Thanks Hui for the clarification

Best Regards,

Puspam N

0 Kudos
Reply