Marking Code explain request

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Marking Code explain request

17,553 次查看
andreagaluppi
Contributor II

Hello,

please could you help me to understand this marking code below present onto MKE02Z64VLC4 body part

M2Q6 VLC4 2N22J CTDEEG

is there a datacode ?

is there a lot nr ?

is there a document that could explain this ?

thanks and regards

Andrea

标签 (1)
4 回复数

15,050 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Andrea,

I will show you the mean of the KE series product number scheme, and the 2N22J stand for the mask number.

Then you can get to know what exactly chip you use after you have the information of product and mask number.

MKE02Z16VLC2M02Q4VLC
MKE02Z16VLC4M2Q4VLC4
MKE02Z32VLC2M02Q5VLC
MKE02Z32VLC4M2Q5VLC4
MKE02Z64VLC2M02Q6VLC
MKE02Z64VLC4M2Q6VLC4
MKE04Z8VFK4M04Q3V
MKE04Z8VTG4M04Q3VTG


Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

13,075 次查看
Edgar_Jiang
Contributor II

hi,I  have a confusion about the marking.Why the marking of two components from the same package have a different marking? The part number is  S9S12G64AMLF.

Edgar_Jiang_0-1649674789585.pngEdgar_Jiang_0-1649674789585.png

 

 

0 项奖励
回复

13,718 次查看
isagani
Contributor III

Please advise what is the date code for the top marking "XNAQ0Q" for the part number MKE02Z64VLC4? Thanks.

Top Marking:

1st line: M2Q6
2nd line: VLC4
3rd line: 2N22J
4th line: XNAQ0Q

 

isagani_0-1635824827694.pngisagani_0-1635824827694.png

 

 

标记 (1)
0 项奖励
回复

15,050 次查看
andreagaluppi
Contributor II

Thank you so much ☺

Cheers

Andrea

0 项奖励
回复