MY FRDM-K64F doesn't work

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MY FRDM-K64F doesn't work

1,417 Views
cyx
Contributor I

it is the first time i use this board. After being connected with computer by USB, the RGB LED keeps flickering and the teraterm can't show any character string even after modify the configration.

And after build a project in KDS, I can't debug. It always shows an error as follow:

An internal error occurred during: "Launching LED_Debug_OpenOCD".

ilg.gnuarmeclipse.debug.gdbjtag.dsf.GnuArmServicesFactory.<init>(Ljava/lang/String;Ljava/lang/String;)V

could someone help me? I'm new to this development board

0 Kudos
Reply
1 Reply

1,307 Views
ivadorazinova
NXP Employee
NXP Employee

Hi yx chen,

thank you for your feedback.

Please, see this post​ if you don´t have issue with the GNU ARM Eclipse plugin.

For this case is needed to replace original files. It is known issue, for this moment it is a workaround.

For your first steps I can recommend you:

Kinetis Design Studio Videos, Part 1: Installation of KDS and Kinetis SDK

Kinetis Design Studio Videos, Part 2: Installation of OpenSDA Firmware on Freedom Board

Kinetis Design Studio Videos, Part 3: Debugging with Kinetis Design Studio

Kinetis Design Studio Videos, Part 4: Using Processor Expert in KDS

Please let me know, if this helps you.

Best Regards,

Iva

0 Kudos
Reply