MRB-KW019032NA interface to Raspberry Pi

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MRB-KW019032NA interface to Raspberry Pi

1,366 Views
aliasgharrajabi
Contributor I

I have a MRB-KW019032NA and am trying to connect to my Raspberry Pi through UART interface. It is supposed to receive signals from a FXTH870511 TPMS sensor and pass them over to Pi.

In MRB-Kw01 manual it says how it could be mounted on a TWR-RF board and how jumper setting should change (relative to the standalone case). Now I would like to do the same thing with Raspberry Pi instead of TWR-RF and I wonder if anybody here has experience to help me. Thanks alot.

Tags (2)
0 Kudos
Reply
1 Reply

1,292 Views
gerardo_rodriguez
NXP Employee
NXP Employee

Hello Aliasghar,

You can take a look at the MRB-KW0x Schematic and the TWR-RF schematic in the TWR-RF Module Reference Manual to see how the connections are being made between both boards. From the MRB-KW0x board headers you should be able to get access to the UART signals.

Regards,

Gerardo

0 Kudos
Reply