MQXLite current datetime/localtime

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MQXLite current datetime/localtime

1,542 次查看
srividhyaumasha
Contributor I

I am trying to get the local datetime in a mqxlite project using code warrior 10.6.   I do not want to use a NTP Server.

* I was using time.h, with a baseboard project. Unfortunately i don't think the implementation is available with kinetics.

* Tried _time_ticks_to_xdate - Could not trace the header.

in vain

Is there anyone who can help me get the current date/time.

标签 (1)
0 项奖励
回复
1 回复

1,351 次查看
ivadorazinova
NXP Employee
NXP Employee

Hello Srividhya Umashanker,

you can set it i.g. by this way:

void setTime(uint16_t year, uint16_t month, uint16_t day, uint16_t hour, uint16_t minute, uint16_t second, uint16_t timezone)

{

    TIME_STRUCT  timeStruct;

    DATE_STRUCT dateStruct;

    MQX_TICK_STRUCT_PTR ticks;

    uint32_t      rtc_time;

    ticks = _mem_alloc(sizeof(MQX_TICK_STRUCT_PTR));

    dateStruct.YEAR = year;

    dateStruct.MONTH = month;

    dateStruct.DAY = day;

    dateStruct.HOUR = hour;

    dateStruct.MINUTE = minute;

    dateStruct.SECOND = second;

    dateStruct.MILLISEC = 0;

            if ( _time_from_date(&dateStruct, &timeStruct) == FALSE)

            {

                        printf("\n Cannot convert date_time ");

            }else{

                        rtc_time = timeStruct.SECONDS;

                        _time_set(&timeStruct);

                        _rtc_set_time(rtc_time);

                        _time_get_ticks(ticks);

                        _time_add_hour_to_ticks(ticks,timezone);

                        _time_set_ticks(ticks);

            }

}

I hope it helps,

Iva

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复