MKW36 LVD interrupt

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MKW36 LVD interrupt

3,054 次查看
842203661
Contributor II

hello,

      I have a question about LVD for MKW36A512:

      When I enable the interruption and disable the reset function of LVD, the decrease of VDD voltage can trigger LVDF setting, but it will not trigger LVD_LVW_DCDC_IRQHandler Call.Why?

      Thanks in advance.


void board_lvd_config(void)
{
    PMC->LVDSC1 = PMC_LVDSC1_LVDV(1);
    PMC->LVDSC1 |= PMC_LVDSC1_LVDACK(1);
    PMC->LVDSC1 | PMC_LVDSC1_LVDRE(1);

    PMC->LVDSC2 = PMC_LVDSC2_LVWV(1);
    PMC->LVDSC2 |= PMC_LVDSC2_LVWACK(1);
    PMC->LVDSC2 |= PMC_LVDSC2_LVWV(1);
}

标签 (1)
0 项奖励
回复
2 回复数

2,970 次查看
nxf63973
NXP Employee
NXP Employee

Hi Luo Liang

 

I cannot see in the function you posted the setting of the LVD Interrupt Enable bit and the enabling of the corresponding interrupt request in the NVIC module. Could you please confirm if these settings are in another part of your program?

 

Also, please take into consideration that the LVD Reset Enable bit is a write-once bit. Once you made a write on PMC_LVDSC1 register you would not be able to change the configuration of this bit until the next reset.

 

Please let me know if you need any more information.

 

Regards

Jose

0 项奖励
回复

2,970 次查看
842203661
Contributor II

Thanks! I forgot to configure NVIC。