MKW31Z512 SWD pin disable

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MKW31Z512 SWD pin disable

ソリューションへジャンプ
2,583件の閲覧回数
Angletown
Contributor I

Hi 

 

In the K32W061/K32W041 User Manual (https://www.nxp.com/docs/en/user-guide/UM11323.pdf) it is mentioned how to setup the MCU to disable SWD at boot.

 

I cannot seem to find similar information about the MKW41Z/31Z/21Z, specifically the MKW31Z (https://www.nxp.com/docs/en/data-sheet/MKW41Z512.pdf). Is it the same/other procedure, or is it not an available feature for the MKWX1Z family?

Thanks

ラベル(1)
0 件の賞賛
返信
1 解決策
2,565件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi @Angletown,

I hope you are doing great.

The K32W and KW31, in this case, are completely different.

However, you could disable the SWD pins, you could create a routine that selects a different pin functionality in those pins.

Remember, it will be a problem to connect with the debugger after you have disabled the pins.

I am not sure if you want to protect your memory flash, but you could look at the next AN.

https://www.nxp.com/docs/en/application-note/AN4507.pdf

Regards,

Mario

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,566件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi @Angletown,

I hope you are doing great.

The K32W and KW31, in this case, are completely different.

However, you could disable the SWD pins, you could create a routine that selects a different pin functionality in those pins.

Remember, it will be a problem to connect with the debugger after you have disabled the pins.

I am not sure if you want to protect your memory flash, but you could look at the next AN.

https://www.nxp.com/docs/en/application-note/AN4507.pdf

Regards,

Mario

0 件の賞賛
返信