KW40Z_Connectivity_Software_1.0.1 (KSDK_1.3.0); IAR 7.50;
I'am trying to setup one capacitive button touch using TSI engine.
located on TSI0_CH15 on my MKW30Z
39 28 PTC3 DISABLED TSI0_CH15 PTC3/LLWU_P11 RX_SWITCH I2C1_SDA UART0_TX — — DTM_TX
As reference I used:
frdm_kw40z_demo_1.0
frdm_kw40z_demo_1.0\source\sensor_drivers\tsi_sensor\ tsi_sensor.h and tsi_sensor.c
I modified:
tsi_sensor_electrode_data_t tsiSensorElectrodeList[] = {
{
.channel = 15,
},
};
change configure_tsi_pins(0);
PORT_HAL_SetMuxMode(PORTC,3u,kPortPinDisabled); /* TSIO_CH15 */
but it get stuck in TSI_DRV_Measure(0) after initialization ?
tsi_sensor_status_t tsi_sensor_start_single_measurement (void){
tsi_status_t result;
/* Start measurements */
result = TSI_DRV_Measure(0);
....
MKW30Z4_features.h
/* @brief TSI module version. */
#define FSL_FEATURE_TSI_VERSION (4)
I presume that is used fsl_tsi_v4_hal_specific.h, fsl_tsi_v4_driver_specific.c
\KW40Z_Connectivity_Software_1.0.1\KSDK_1.3.0\platform\drivers\src\tsi
Some other changes are necessary ?
There is some relations with TMR or TPM set-up ?
Best Regards,
Lucian