MKW30Z Total number of timers

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MKW30Z Total number of timers

626 次查看
lucianfiran
Contributor V

KW40Z_Connectivity_Software_1.0.1 KSDK_1.3.0 IAR 7.5

I see that the total number of timers defined as:

gTmrTotalTimers_c   ( gTmrApplicationTimers_c + gTmrStackTimers_c )

in TimersManager.h

In examples I see these numbers (app_preinclude.h)

/* Defines number of timers needed by the application */
#define gTmrApplicationTimers_c         4

/* Defines number of timers needed by the protocol stack */
#define gTmrStackTimers_c               5

First, there is a total max number of timers ?

If I add TPM channels for PWM like al this 5
TPM1_CH0, TPM1_CH1, TPM0_CH0, TPM0_CH1, TPM0_CH2

Do I need to increase number of timers needed by the application ?

Thank you,

Lucian.

标签 (1)
标记 (3)
0 项奖励
回复
0 回复数