MKV56F512VLL20

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MKV56F512VLL20

1,267 Views
erskineb
Contributor I

Can anyone please post a link for initialization code for a MKV56F512VLL20? It is not listed in Processor Expert.  A project that can be imported into IAR would be great. I have found several locations on the Freescale Website that indicated its presents, but nothing there.

Labels (1)
0 Kudos
Reply
1 Reply

1,095 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Erskine,

I've attached the startup and liker files of the KV31 instead of the KV56 , and you can port these files to the KV56 easily.

Hope it helps.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply