MKV56F512 Pin Muxing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,805件の閲覧回数
derekcook
Senior Contributor I

Hello,

There is a shortage of the MKV31. Due to this, we are switching to the MKV56 100 pin package which looks to be a pin match to the MKV31. We only have a conflict with 1 pin. On pin 4 we need SPI1_SOUT and only SPI1_SIN is listed. Is maybe ALT_MUX7 missing in the datasheet?

 

derekcook_0-1655140889389.png

 

 

On the MKV31 ALT_MUX7 allowed us to assign this pin to SPI1_SOUT

derekcook_1-1655140889415.png

 

 

Thanks for your help!

0 件の賞賛
返信
1 解決策
1,799件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @derekcook 

The data sheet is correct, looking at the pin configuration for the SPI1_SOUT you only can use pins number 2, 62 and 99

 

B.R.

VaneB

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,795件の閲覧回数
derekcook
Senior Contributor I

Thanks VaneB! This resolves my question. 

0 件の賞賛
返信
1,800件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @derekcook 

The data sheet is correct, looking at the pin configuration for the SPI1_SOUT you only can use pins number 2, 62 and 99

 

B.R.

VaneB

0 件の賞賛
返信