MKV56F1M0VLQ24

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MKV56F1M0VLQ24

1,212 Views
tangliyusky
Contributor I

Hi:

      The MKV58F1M0VLQ24 and MKV56F1M0VLQ24,the two Chip compatible?If I dont need Ethernet,the MKV56F1M0VLQ24 can replace MKV58F1M0VLQ24?

0 Kudos
Reply
1 Reply

1,106 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I think that the KV56 and KV58 are  pin to pin compatible for corresponding package, the only difference is that KV56 does not have Ethernet module and only have 2 CAN modules, while the KV58 has one Ethernet and 3 CAN modules.

Hope it can help you

BR

Xiangjun Rong

pastedImage_1.png

0 Kudos
Reply