MKM34Z256 SDK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MKM34Z256 SDK

2,623件の閲覧回数
kamilpiekos
Contributor I

Hello,

I have a question, I started working on TWR-KM34Z75M with MCUXpresso and with that i got SDK in version 2, but when I got METERLIBFFT r4, I noticed inside this lib drivers are in version 1. And right now I'm not sure if I downloaded wrong version of meterlibfft, or it's not ported to SDK2 ?

Thanks in advance,

Kamil

タグ(1)
0 件の賞賛
返信
3 返答(返信)

2,320件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Kamil,

   Thank you for you updated information.

   I checked the lib which in the post, that code structure is not the SDK structure, it should be the register control driver, this KM34 driver is easy to understand, please note, the project used chip is Freescale MKM34Z128xxx5.

  I think you can refer to that application software, you don't need to use the SDK, but if you want to use the SDK, you need to do the porting by yourself.


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,320件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Kamil,

     Please tell me where you download the METERLIBRRT r4? Please give me your download link from the NXP, then I need to check it at first.

    If the lib is very old, it may use the old SDK driver.

     But, now if you want to use the SDK, I highly suggest you use our newest SDK code for your KM34.


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,320件の閲覧回数
kamilpiekos
Contributor I

Hey Kerry,

I got meterlib from https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fwww.nxp.com%2Fwebapp%2FDownload%3Fcol... according to this post https://community.nxp.com/thread/476360 

So I should use newest SDK (2.2) with this meterlibfft r4, right ?

 

Kamil

0 件の賞賛
返信