MKM34Z256 Comparator input impedance

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MKM34Z256 Comparator input impedance

ソリューションへジャンプ
2,528件の閲覧回数
petr_uhlir
NXP Employee
NXP Employee

Dear Colleagues,

our customer wants to use MKM34 comparators in their application  And there is question they didn’t find the answer in the documents:

They want to use the three high speed comparator modules in the KM34Z256 to detect an overcurrent as fast as possible. (one for each phase). To connect our external circuit to the comparator input, they must know their input impedance. If the impedance of the comparator inputs is as low as the ADC inputs (some kOhm) than they must add separate impedance converter.
If the input is like a CMOS-Comparator (several MOhm) then the impedance converters are not needed.

Can you tell me the input impedance of the comparator inputs?

Thank you and kind regards,

Petr

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,374件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hi Petr,

 

I received information from the design team:

 

The answer is impedance <5K ohm after checking with IP owner.

 

Best regards,

Felipe

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,375件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hi Petr,

 

I received information from the design team:

 

The answer is impedance <5K ohm after checking with IP owner.

 

Best regards,

Felipe

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
2,374件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hi Petr,

I just asked the design team about this parameter. I will let you know as soon as I have any update.

Best regards,

Felipe

0 件の賞賛
返信