MKM34256 cannot pass oscillator initialization

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MKM34256 cannot pass oscillator initialization

2,422 Views
martinzhang
Contributor III

Hi

There is a batch of MKM34256 work well for a long time, but few of them got a problem which the oscillator cannot be initialized correctly sometime. The code is stuck in following line:

 

if (MCG_C2 & MCG_C2_EREFS0_MASK) { WAIT_FOR_FLAG (MCG_C2, EREFS0, OSCINIT0); }

 

Please let me know if you know the reason of this issue.

Thank you very much!

Martin

Labels (1)
0 Kudos
Reply
3 Replies

2,402 Views
diego_charles
NXP TechSupport
NXP TechSupport

Hello @martinzhang 

I hope you are doing well!

From the description,  it seems that the external crystal/resonator  is not being able to get the sufficient stability or number of clock cycles in certain units. See this section below.

diego_charles_0-1627963754938.png

I am thinking in the following things:

What is the frequency of your external crystal or resonator? This to will also give us opportunity to review the oscillator circuitry according to Table 36-2  of the RM.

 When the MCU gets stop at oscillator initialization ,  did it have  low power mode setting/transition ; transition of MCG mode ; or was coming out of a  Power on cycle?

This app note Crystal Oscillator Troubleshooting Guide  could also be worthy for our trouble shooting task  . Here is an excerpt , that is related to the hypothesis that I mentioned above.

diego_charles_1-1627964939299.png

Please accept my apologies for the delay

Diego.

 

 

 

 

 

 

 

0 Kudos
Reply

2,388 Views
martinzhang
Contributor III

Hello Diego,

Thank for your reply and this is very helpful.

Following is the crystal circuit.

martinzhang_0-1627969156105.png

 

Now, all the devices work well and I will check it when this issue come again.

 

Best Regards,

Martin

 

0 Kudos
Reply

2,385 Views
bobpaddock
Senior Contributor III

If the 22 pF capacitors and all the layout parasitics balance out perfectly such a circuit will not start, the 1M resistor is there to fix this.
The odds of this are small, except for Murphy's Law saying otherwise.

If it continues to be a problem replace one of the caps with one of a slightly different value.
Some chips have internal caps that can be enabled.  Don't enable those at the same time as external ones.

The caps should match the loading specified by the crystal manufacture.




0 Kudos
Reply