MKM34 and MKM35 code compaitbility, one code for both controllers

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MKM34 and MKM35 code compaitbility, one code for both controllers

ソリューションへジャンプ
3,062件の閲覧回数
Chris_P
Contributor I

Hello *,

I have the case that I want to replace the MKM34Z256 with the MKM35Z256 and I only use those internal modules and features that both of them have inside. 

Is it possible to compile the code only for the MKM35 and run it on both controllers without any risk? (watchdog is active) I have already run code compiled for 34 on the 35 without any obvious problems...

As I read in the docu and migration guide there are only small additions in the MKM35, they have the same pinning, registers, adcs etc and even the SDK drivers I use in Keil are nearly the same, only minor differences.

 

Thanks in advance !!

Christian

タグ(3)
0 件の賞賛
返信
1 解決策
3,025件の閲覧回数
RaRo
NXP TechSupport
NXP TechSupport

Hello @Chris_P,

Is it possible to compile the code only for the MKM35 and run it on both controllers without any risk?

As you mention, both microcontrollers share some characteristics and functionalities.

Nonetheless, you should be careful with those that are not, for example: SRAM. Specially if you intend to program or compile from MKM35Z256 to MKM34Z256.

You could continue working as you mention, but it might be a better practice to use the corresponding microcontroller SDK.

Best regards, Raul.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,537件の閲覧回数
amal_s
Contributor I

Hi Chris_P,

Can you tell which compiler are you using for code?

If it is IAR, which version?

Are you able to build output file for both MKM34Z256 and MKM35Z256 using IARv9.10.2?

I'm facing a issue while compiling the code for MKM34Z256 with iarv9.10.2. I think some linker issues.

The error shown is: Fatal Error[Lp049]: there was no reference to __iar_data_init3, but it is needed to initialize section .bss (irtc.o #8) on iar v9.10

can you please help me if you have any idea regarding this error, I'm new in this field:(

Thanks and regards

0 件の賞賛
返信
3,026件の閲覧回数
RaRo
NXP TechSupport
NXP TechSupport

Hello @Chris_P,

Is it possible to compile the code only for the MKM35 and run it on both controllers without any risk?

As you mention, both microcontrollers share some characteristics and functionalities.

Nonetheless, you should be careful with those that are not, for example: SRAM. Specially if you intend to program or compile from MKM35Z256 to MKM34Z256.

You could continue working as you mention, but it might be a better practice to use the corresponding microcontroller SDK.

Best regards, Raul.

0 件の賞賛
返信
3,002件の閲覧回数
Chris_P
Contributor I

Hi Raul,

thank you for your reply and your hint regarding the SRAM, to be honest I didn't recognize the different address ranges in MKM34 and 35.

I will reconsider the one-compile-for-all strategy

 

Best regards,

Christian 

0 件の賞賛
返信