MKM33 AFE Modular

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MKM33 AFE Modular

1,875 Views
huasu
Contributor I

use AFE module, found that the voltage input differential voltage and the calculated value is different, the difference of about 13%. For example, into a differential signal 200mV, read out from the results of balance device value is 3175931, then the calculated results should be 227mv (3175931/8388607 (0x7FFFFF) * 600 (MV) = 227mv), so the measured value is 227mv butinto value is 200mv. and therefore the result is wrong. Don't know why

Tags (1)
0 Kudos
Reply
2 Replies

1,736 Views
Paul_Tian
NXP Employee
NXP Employee

Hi, Su Hua

Would you please help to show how do you check the analog voltage value? Do you use times measurement and calculate average value? You can use hardware average function.

Best Regards

Paul

0 Kudos
Reply

1,736 Views
huasu
Contributor I

Hi, Zhe Tian

I have no found‍ hardware average function in the afe modular.thanks

0 Kudos
Reply