MKM33 AFE Modular

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MKM33 AFE Modular

1,782件の閲覧回数
huasu
Contributor I

use AFE module, found that the voltage input differential voltage and the calculated value is different, the difference of about 13%. For example, into a differential signal 200mV, read out from the results of balance device value is 3175931, then the calculated results should be 227mv (3175931/8388607 (0x7FFFFF) * 600 (MV) = 227mv), so the measured value is 227mv butinto value is 200mv. and therefore the result is wrong. Don't know why

タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,643件の閲覧回数
Paul_Tian
NXP Employee
NXP Employee

Hi, Su Hua

Would you please help to show how do you check the analog voltage value? Do you use times measurement and calculate average value? You can use hardware average function.

Best Regards

Paul

0 件の賞賛
返信

1,643件の閲覧回数
huasu
Contributor I

Hi, Zhe Tian

I have no found‍ hardware average function in the afe modular.thanks

0 件の賞賛
返信