MKM14Z64ACHH5 Is the mass-erase function implemented?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MKM14Z64ACHH5 Is the mass-erase function implemented?

Jump to solution
2,285 Views
jun1
Contributor V

Hi.

kinetis-KM series MKM14Z64ACHH5 Is the mass-erase function implemented?
As IAR's EWARM flash loader option setting does not enable mass flashing before flash writing, I was worried that the device does not have that function.

Thank you.

0 Kudos
Reply
1 Solution
2,178 Views
miduo
NXP Employee
NXP Employee

Hello,

Sorry for the late response.

Answer to your question, the mass-erase function surely implemented. Do not worry. You may do like below:

Untitled.jpg

View solution in original post

2 Replies
2,178 Views
jun1
Contributor V

thank you for your answer.
OK. It was good.

0 Kudos
Reply
2,179 Views
miduo
NXP Employee
NXP Employee

Hello,

Sorry for the late response.

Answer to your question, the mass-erase function surely implemented. Do not worry. You may do like below:

Untitled.jpg