MKM14Z64ACHH5 Is the mass-erase function implemented?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MKM14Z64ACHH5 Is the mass-erase function implemented?

ソリューションへジャンプ
2,281件の閲覧回数
jun1
Contributor V

Hi.

kinetis-KM series MKM14Z64ACHH5 Is the mass-erase function implemented?
As IAR's EWARM flash loader option setting does not enable mass flashing before flash writing, I was worried that the device does not have that function.

Thank you.

0 件の賞賛
返信
1 解決策
2,174件の閲覧回数
miduo
NXP Employee
NXP Employee

Hello,

Sorry for the late response.

Answer to your question, the mass-erase function surely implemented. Do not worry. You may do like below:

Untitled.jpg

元の投稿で解決策を見る

2 返答(返信)
2,174件の閲覧回数
jun1
Contributor V

thank you for your answer.
OK. It was good.

0 件の賞賛
返信
2,175件の閲覧回数
miduo
NXP Employee
NXP Employee

Hello,

Sorry for the late response.

Answer to your question, the mass-erase function surely implemented. Do not worry. You may do like below:

Untitled.jpg